AXIS#.PL.ERRFTHRESH

Description

This parameter sets the maximum position error. If the position error AXIS#.PL.ERR is larger than AXIS#.PL.ERRFTHRESH the drive generates a fault. If AXIS#.PL.ERRFTHRESH is set to 0, the maximum position error is ignored.

Example

Set position rotary units to 2 (degrees). Setting AXIS#.PL.ERRFTHRESH to 1000 states that is the position error is larger than 1000 degrees, the drive will generate a fault.

AXIS#.UNIT.PROTARY 2
AXIS#.PL.ERRFTHRESH 1000

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

42949672960 counts

Note: Default is adjusted to account for the units selected by the user

Data Type

Float

See Also

AXIS#.PL.ERR
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
AXIS1.PL.ERRFTHRESH

500ch

03h

Signed32

Position

-

Read/Write

No

AXIS2.PL.ERRFTHRESH

510ch

03h

Signed32

Position

-

Read/Write

No

AXIS1.PL.ERRFTHRESH

6065h

00h

Unsigned32

Position

-

Read/Write

No

AXIS2.PL.ERRFTHRESH

6865h

00h

Unsigned32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.ERRFTHRESH

5902

170E

Signed32

Read/Write

Position

AXIS2.PL.ERRFTHRESH

71438

1170

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.ERRFTHRESH

5902

Signed32

Read/Write

Position